EmployeInfo Service
You have created a service.
To test this service, you will need to create a client and use it to call the service. You can do this using the svcutil.exe tool from the command line with the following syntax:
svcutil.exe https://magshare.in.abb.com/EmployeeInfo.svc?wsdl
You can also access the service description as a single file:
https://magshare.in.abb.com/EmployeeInfo.svc?singleWsdl
This will generate a configuration file and a code file that contains the client class. Add the two files to your client application and use the generated client class to call the Service. For example:
C#
class Test
{
static void Main()
{
EmployeeInfoClient client = new EmployeeInfoClient();
// Use the 'client' variable to call operations on the service.
// Always close the client.
client.Close();
}
}
Visual Basic
Class Test
Shared Sub Main()
Dim client As EmployeeInfoClient = New EmployeeInfoClient()
' Use the 'client' variable to call operations on the service.
' Always close the client.
client.Close()
End Sub
End Class